This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478: 启动电流太大

Part Number: LM3478
Other Parts Discussed in Thread: TPS40211, LM5121

我用 WEBENCH Power Designer构建了5~9V(实际应用为7.2V充电电池)输入,输出80V0.2A的电路如图所示:

实际应用中发现电池和小功率稳压电源不能顺利启动,并且MOS管烫到可以熔掉焊锡,但是使用大功率稳压电源则可以顺利启动。在电池应用中电池后期可能很难维持3A以上的启动电流,请看有什么什么办法调整?或者给替代型号(可以重新设计电路板)?我在TI官网查找了方案,用TPS40211之类的,需要一个非常大的电感,比如190uH 8.2A,市面上如此大容量大电流的功率贴片电感