你好,在ucc28950的datasheet中,提到Ucc28950的变压器占空比最大可设置到70%(P.39),在TIDA-020031中甚至可以达到90%(P.5),请问这样不会使上下桥臂导通损坏吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
见芯片datasheet第六页参数表最大duty 典型值是95%, 或者看datasheet Figure 10.
datasheet中提到的70%是这个设计案例推荐在最小输入电压时的最大duty值为70%(只是针对这个案例,实际上duty可以更大)。
HI
单个驱动输出见芯片datasheet第六页参数表最大duty 典型值是95%。