This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951-Q1: 开发一款移相全桥升压DC-DC电源,同步整流占空比丢失严重。

Part Number: UCC28951-Q1
Other Parts Discussed in Thread: PMP8740

Hi all:

        我使用UCC28951-Q1来搭建一台24V升压至48V的DC-DC电源,电路参考了PMP8740中的拓扑图。

        目前测试时发现,当我使用同步整流控制次级MOS管开关时会有严重的占空比丢失现象,次级线圈几乎有一半的时间处于短路状态,导致电压无法升到设定值。

        当我使用二极管替换同步整流MOS时,输出电压可以升压到设定值。

        如下波形可以说明此种情况,我想知道UCC28951-Q1是否有升压应用的方案可供参考,以上问题有无调整的方法。谢谢!