Part Number: TPS54302
设计的24V转5V的DC/DC电路, 本来打算输出的5V 再通过dc/dc 用来生成4G模组使用的3.8V
现在总电源输入降到5V以后, 后一级DC/DC的供电会变成怎么样? 如果输入5V,经过TPS54302的5V输出电路 实际输出是多少?
能否提供2A的电流能力?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS54302
设计的24V转5V的DC/DC电路, 本来打算输出的5V 再通过dc/dc 用来生成4G模组使用的3.8V
现在总电源输入降到5V以后, 后一级DC/DC的供电会变成怎么样? 如果输入5V,经过TPS54302的5V输出电路 实际输出是多少?
能否提供2A的电流能力?
翻译
搜索
复制
HI
你的意思是24V降低到5V吗? 如果5V给到TPS54302, 他的输入5V将会在100%duty下工作,即便如此因为有MOS, 电感等损耗,输出电压将会低于5V.
如果降低到4V多 , 影不影响2A的输出能力?
翻译
搜索
复制
Hi
电流不影响,建议直接24V转换到3.8V, 如果需要5V再做一个转换。