Other Parts Discussed in Thread: TUSB1064
I had set the tps65987 with GUI. the But that triggering event doesn't take effect。I use the tps65987's gpio control tusb1064 (not through i2c). the ctl1,ctl0,flip which 3 pins can't flip when I flip the type-c line(the tps65987 pins is gpio0 gpio1 gpio2). my borad function is use alt mode for 2 lanes DP, and USB3.1. don't use PD for power manage. can you provide a code project ,or configure set with GUI. I can't success with many days, our time is very tight。 very thanks . I set as the picture, I don't know how to set other option,or this is a wrong set。