Hello!
TIDA-01494,this scheme is for 24V 20A output. I want to turn it into a 48V20A output.
I have doubled the number of secondary turns on the transformer. Besides, what other changes do I need to make?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
TIDA-01494,this scheme is for 24V 20A output. I want to turn it into a 48V20A output.
I have doubled the number of secondary turns on the transformer. Besides, what other changes do I need to make?
HI
你这个已经相当于要重新设计了,除了匝比,变压器感量,反馈等等都是要重新设计的。建议按照datasheet里面的案例重新计算设计。
I have now doubled the secondary side of the transformer. If I disconnect the feedback, I can output 48 V , but If feedback is connected, the output is still only 24 V . I know there was a problem with the feedback, but I won't make any changes. Could you please give me some suggestions ,Thanks