Part Number: TPS62A01A
Other Parts Discussed in Thread: TPS62A01
请问:
按照datasheet table9-3,电感的典型值为1uH。
如果在输出端额外增加LC滤波电路,那么电感的感值改如何选择?是否L1+L2应该为1uH ?或者是不用考虑L2的感值,L1为1uH即可?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
TPS62A01的电路按照datasheet来设计即可,与后面的LC无关,同样LC也即是单独设计与前面DC/DC无关,一般LC, L选用电流足够的磁珠,C选择10~47uF是可以的。
你好,请问后面的L2的取值为什么与1uF无关?理论上看,无论后级使用磁珠+电容(磁珠也有等效电感)还是电感+电容,整个回路的总电感是L2+L1.
Ton期间:Vsw-Vo=(L1+L2)di/dt
Toff器件:Vo=(L1+L2)di/dt
Vo为固定输出电压,L2的存在会使纹波电流变小。
但是,L2的存在导致了总电感L2+L1>1uF,是否会带来新的问题?
HI
这完全是两级电路,前面的DC/DC是功率转换,后面的LC是滤波。