Other Parts Discussed in Thread: UCD9222, UCD74120, UCD74106
专家你好:
最近在调试自己做的C6670的板子,上面的电源方案是照搬C6670开发板上面的电路,使用UCD9222+74111+74106分别产生可调0.9-1.1V和固定1V的电源。现在遇到如下问题:
用Fusion 软件对UCD9222进行配置,无论是使用开发板的配置程序还是使用自己设计的配置程序,74111都有输出,但74106均无输出,一点击使能就出现FLT错误,但我不知道究竟是哪里出现的错误。我将自己的配置程序加载到开发板是可以正常运行的,表明程序应该没什么问题。我想在软件Configuration里面屏蔽错误控制字,发现没有效果。而且测量74106的FTL输出是为低电平,所以我估计是不是UCD9222的CS测量发现电流有问题就报了这个错误?或者说会不会是74106这个芯片有问题?另外问一个问题,CS管脚要测量电流值得话是要配置电流增益和偏置的值,我是按照开发板程序中的值进行配置的,不知道是否可行?还是与具体硬件电路有关?最后将Monitor中的截图放在这里,希望能够对您分析错误有所帮助。