https://www.ti.com.cn/tool/cn/PMP30339?keyMatch=LM5141在使用LM25141参考连接设计一款24V输入,12V20A输出的电源。输出电感L4用5.6uH,输出限流电阻R10用2mR。测试过程中,输入功率足够情况下,输出电流大于8A,电感就开始啸叫,输出电压开始变得很不稳定~一点几伏到八点几伏跳变。当把电流采样电阻到芯片CS引脚的电阻R16焊掉,电流很轻松就可以去到20A。采样电阻R10改为1.5mR输出电流也是只能最高8A。请问这是什么问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
https://www.ti.com.cn/tool/cn/PMP30339?keyMatch=LM5141在使用LM25141参考连接设计一款24V输入,12V20A输出的电源。输出电感L4用5.6uH,输出限流电阻R10用2mR。测试过程中,输入功率足够情况下,输出电流大于8A,电感就开始啸叫,输出电压开始变得很不稳定~一点几伏到八点几伏跳变。当把电流采样电阻到芯片CS引脚的电阻R16焊掉,电流很轻松就可以去到20A。采样电阻R10改为1.5mR输出电流也是只能最高8A。请问这是什么问题
Hi
应该是引起了不稳定导致电感提前饱和。
TI提供的参考设计一般都是有做成板子测试没有问题的,之所以出现问题,可能和CS的layout有关。如上如果将R16去掉,是可以达到20A稳定输出,做此修改是没有问题的。