您好,我使用Bq76920采集芯片,采集4串18650单体电压,其中 Bq76920的VC3和 VC4短接。调试中有如下几个问题:
问题1:当我未接入单体电压采集线时,采集芯片可以读取到单体电压的数据,并实时刷新,当然此数据是假的,正常的话不应该读取到的单体电压都为0才对吗
问题2:接入4串单体电压采集线后,当每串单体电压小于大约2.8V时,每节采集到的单体电压数据大约相差30-40mv左右,而当单体电压较大时,一二节电芯单体数据采集偏差很大,比如第一节电芯电压为800mv,第二节电芯电压为7000mv,第三,第四节电芯采集相对正确,但有100mv左右的误差,但是将每节电芯的电压加起来得到的总压数据是正确的。此外,在我们只接第1,2,3节电芯进行采集时,前三节电压都可以采集到相对正确,但误差在100mv左右。而将最后一节电芯接入时,又出现一二节电芯单体数据采集偏差很大的情况。
问题3:当采集芯片报出欠压或过压故障时,要使用主控对它进行复位恢复,是将 SYS_STAT的对应故障位置1来恢复吗
Bat_VOL为总压14.31V
Cell_1,Cell_2,Cell_3,Cell_4 为单体电压
四节电芯的实测电压为3.57V左右,此外,每次重新上电的时候,检测到的单体电压都不一样