This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951-Q1: 同步整流不可用

Part Number: UCC28951-Q1

你好,我现在在做一款移相全桥电路,使用的是TIDA-020031参考设计,设计输出电压20V,电流150A,最大功率3000W。

变压器匝比8:1,谐振电感6uH,变压器漏感1.5uH,输出电感3.3uH,使用倍流整流方案。

现在的问题是,禁用E、F输出时,能够正常输出,电压最大到19V,电流最大到140A,最大功率2700W以上。但是启用同步整流之后,电压升到6V以后,无法继续上升,此时电流大约为40A,我的DCM模式分压电阻分别为15k和560Ω。似乎是因为E、F开始输出信号时副边被整流MOS管短路导致。死区时间设置Rab=Rcd=13k,采用自适应死区时间,电阻网络详见插图。请帮我解决这个问题,我应该从哪个方面调整?