This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMB1428Q: 单独使用该芯片

Part Number: EMB1428Q

hi,

   目前在单独使用emb1428时,在while中调用开关闭合的函数接口,可以正常控制开关的开闭,但是把接口放到1ms_task()任务里运行,或者2ms. 10ms. 100ms中,都不能控制开关闭合,这是为什么呀?

  • 您好, the EMB1428 device is intended as a tandem device with the EMB1499 so we have limited support available for this topic. Can you identify if it is possible to follow our reference material for using the EMB1499? 

  • 您好,

           我这边硬件同事没有使用1499芯片,DONE脚和EN脚是做了一个反向,DIR和DIR_RT做了一个反向,反向的意思是当EN脚为高时DONE为低,这样做能否达到1499的作用呢?

  • Thanks for your reply,

    By the way, two EMB1428 are used in this design, without the use of a 1499 chip. The following designs are made for the seven pins:
    DIR and DIR_ RT has made a reverse circuit, and DONE and EN pins have also made a reverse circuit,
    Three FAULT pins are designed as interlocking functions for two EMB1428 chips. Interlocking is for safety reasons. When one EMB1428 is closing a certain channel, the switch controlled by the other 1428 must be fully open. The FAULT0 pin is controlled through GPIO, and the FAULT1 and 2 are connected to GND. This design currently cannot achieve the effect of two chips interlocking under testing.
    XU ,Please give me some guidance, thank you

  • 您好,正在询问更了解这款芯片的TI工程师,稍后回复。

  • 您好,Unfortunately we do not support this device anymore. Please refer to the datasheet online for any queries.