This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: 有时候不能充电

Part Number: BQ24610

一般情况下都是可以充电的,就是在电池电量从100%连续放电到5%时(电池电压从16.6V放电到12.7),接入适配器就不能充电了,边充电边使用的情况下。不知道什么原因。需要等上好几分钟才能充上电。接入适配器的时候也能识别到电源接入,电源也可以从电池供电切换到适配器供电,但是就是不充电,电池一直都在。识别到一次能充上电后,后面怎么接适配器都没问题,都可以充电,后面电池电量继续放电到3%(电池电压12.4V左右)也能识别得到,可以充电。