This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61175: 要求设计2.9-4.2V的单节锂电池输入,12V3A输出的升压线路

Part Number: TPS61175
Other Parts Discussed in Thread: TPS61288

您好:

        我这边需要设计一个升压线路,要求2.9-4.2V的单节锂电池输入,12V3A输出。

我这边初步看TPS61175的规格书感觉像是符合要求的,但是在电路模拟那部分一直说是无法设计的,请问这部分是什么问题?

此外,如果61175无法支持要求的话,请问是否有其他型号能够支持此需求?

望尽快答复,谢谢!

Zero Huang

  • HI

        TPS61175不符合你的设计要求, 按照你的要求2.9-4.2V输入,12V3A输出, 那么输入电流超过13A, 峰值电流在15A,  而TPS61175支持仅仅3A的峰值电流流入。

       你可以看看TPS61288 

        

  • 您好:

        按照您的推荐,我这边使用了TPS61288做升压12V输出,测试升压输出正常;

    但是在应用上,我接入了降压5V输出的LM2676SX-5.0的时候,出现了过载/短路的现象,请问这会是什么问题呢?