Part Number: TPS61175
Other Parts Discussed in Thread: TPS61288
您好:
我这边需要设计一个升压线路,要求2.9-4.2V的单节锂电池输入,12V3A输出。
我这边初步看TPS61175的规格书感觉像是符合要求的,但是在电路模拟那部分一直说是无法设计的,请问这部分是什么问题?
此外,如果61175无法支持要求的话,请问是否有其他型号能够支持此需求?
望尽快答复,谢谢!
Zero Huang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
TPS61175不符合你的设计要求, 按照你的要求2.9-4.2V输入,12V3A输出, 那么输入电流超过13A, 峰值电流在15A, 而TPS61175支持仅仅3A的峰值电流流入。
你可以看看TPS61288