最近在NVR适配poe功能时,TPS23882出现了一个问题。
工作环境:设置的23882工作模式是自动模式,固件版本号是0x7
现象:在相机接入NVR时,有个别相机无法正常供电,我们设备记录到的对应23882端口的历史峰值功率在10~16w,说明在接入瞬间是有供电的。停止供电后,读寄存器得到的class是Class Overcurrent
问题:请问内部固件是否做了功率限制之类的功能,导致超功率端口强制下电?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在NVR适配poe功能时,TPS23882出现了一个问题。
工作环境:设置的23882工作模式是自动模式,固件版本号是0x7
现象:在相机接入NVR时,有个别相机无法正常供电,我们设备记录到的对应23882端口的历史峰值功率在10~16w,说明在接入瞬间是有供电的。停止供电后,读寄存器得到的class是Class Overcurrent
问题:请问内部固件是否做了功率限制之类的功能,导致超功率端口强制下电?
Hi
如果是个别的话,建议确认负载看看(可以对调负载,看是跟着23882走,还是跟着负载走?)
跟着负载走的,但是负载接到其他厂家的poe上是可以正常使用的。固件里面没有做功率限制吗
另外,Rsense电阻接的是0.255Ω会对这个问题有影响么。我看开发之前接的是0.2Ω的,但是由于暂时缺料,无法更换电阻调试
Hi
如果是个别,其他板子用的也是0.225ohm确实正常的。
有没有做上面确认对调负载,看是跟着23882走,还是跟着负载走?