This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170-Q1: LM5170_Q1 通道1接上CSA1 和CSB1 后上电报错,nFault 输出低,VINX 无信号

Part Number: LM5170-Q1


我们做了一块LM5170-Q1的发开发板,目前设置BUCK模式,30V 输入  12V 输出,双相模式。 上电后无电压输出,没有接负载, 检查发现nFault 输出低,VINX 无电压。 经过排查发现只要断开通道1  电流检测的CSA1 与CSB1 后 , 上电就正常了,通过通道2能输出12V。两个通道电路参数都是一样的。 同时我尝试用通道2 的 CSA2与CSB2 接到通道1 的反馈电阻上,也能正常启动。同样的,我把通道1的CSA1 与CSB1 接到通道2的反馈电阻上,依然不能启动,会报错。  也就是说只要通道1的CSA1与CSB1 接反馈信号,就会报错。请问这个问题需要怎么去检查?目前原理图如下:

DC-DC_zhou.pdf