This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: VBUS到PPHV1路径无输出

Part Number: TPS65987D

各位专家好:

我使用TPS65987D搭建了一个快充电路,电路如下。

现在使用外部TypeC适配器供电测试发现,从VBUS到PPHV1电源路径无输出。

测试LDO_3V3、LDO_1V8输出均正常,使用板上CPU读取987D的I2C1能够读取到设备,测试GPIO0为0V低电平。

目前图中的Flash  MX25L12833FM2I-10G内没有配置987D的相关固件文件,挂载的I2C设备内也没有配置文件。

请问各位专家:

在987D第一次使用时,要为先他进行一次配置吗?

若不需要,请专家们帮助检查为何PPHV1没有输出。

期待各位专家的回复,不胜感激!