Part Number: TPS62180
Other Parts Discussed in Thread: TPS54620
射频电源,输入5V转1.8V@6A
选型选了TPS62480RNCR和TPS62180YZFR这两种,BOM价格也差不多,区别是适用电压范围不同
所以想请教一下 一般在选型的时候,在都满足的情况下电压等级选择高的还是低的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
都可以,只要输入电压美国过充,选择5.5V输入都是可以的,没有必要一定选择更高电压如15V输入的。
另外你也可以选择单个电感的设计,例如TPS54620之类。
同时考虑到你用于射频,或对纹波noise如果较敏感的话,可以在输出增加一级LC.