This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5045: 同步驱动不发波

Part Number: LM5045

1. LM5045在应用的时候,出现空载启机SR不发波的情况(SSSR没有充电),只能把环路调很快才会出同步整流,但这不是我们想要的结果。
目前50台样机,出现两台这样的。想知道这是什么原因?
输入电压范围 48V到60V ,匝比4:1,输出11V ,在48V输入的时候也会出现空载启动SR不发波的情况。

2.如下规格书所诉,要满足三个条件,如下红色的PULSE 是指原边驱动,还是哪里呢?