This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC34063A: NE5534x Low-Noise Operational Amplifiers DC-DC Power Solutions

Part Number: MC34063A
Other Parts Discussed in Thread: TPS61093

Hell0! TI Team


We are again looking for a power management solution that supports ±15V supply, this supply is applied to NE5534x Low-Noise Operational Amplifiers, We have looked at the MC34063A and it doesn't seem to be a very good fit. please help to recommend a suitable application solution and reference application design, thanks!

  • Hi

         你的输入电压是多少?  正负电压输出最大电流多少?

  • 您好!

    输入电压是3.3V~4.4V;输出电压是+15V和-15V,因为是给音频运放供电,输出电流不需要很大,50mA内都足够用了。请帮忙推荐一个合适的电源芯片解决方案,注意我的应用是用于音频运放供电,对电源要求非常高,否则很容易出现音频噪音。

  • HI

       可以选择TPS61093等芯片,可以参考datasheet 第16页的电路,或者也可以选择TPS61080/1之类的芯片(datasheet上有推荐电路)

     如你所说,音频运放对纹波noise都很敏感,一般需要在DC/DC后增加LC(磁珠加电容)甚至高PSRR低Noise的LDO.