This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25116: 给电池冲电

Part Number: LM25116


买了LM25116做的300W转换器用16V输入供电降压到12.5 V给电池组充电。

先在输出端接12V 20W卤素灯 调到 12.5V 约 1.5 A 是没有问题的。

但换接约10.5V ( 没冲满的锂电池组 ) 后输出端变为10.5 V但没有冲电电流。

是否给电池充电必须是升降压模块?