This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24196: 应用可行性求助

Part Number: BQ24196
Other Parts Discussed in Thread: TUSB320, BQ24195, TPS2543, BQ24190, BQ25890H, BQ25611D, BQ24392, TUSB320LAI

TI 你好

目前我正在设计一款带有电池和otg功能的控制板,想使用以下几个芯片搭配来实现完整的otg和充电支持

BQ24196--充电ic

TUSB320--cc逻辑芯片,配置为DRP模式,ID通过上拉连接到BQ24196的OTG引脚

目前是仅通过TUSB320的cc逻辑来检测输入电流,但是由于大部分家用充电器都只含有type-A接口,而连接线只有56k的上拉电阻,导致不能通过CC来判断是否能够支持2A电流的输出(也就是说无法在使用A to C线的情况下识别哪个是电脑主机之类的host,哪个是充电器之类的adapter

目前想通过充电器协议的BC1.2之类的,使用D+和D-来检测实际的输出电流限制,但是我的D+和D-被微控制器占用,并且此微控制器不支持上述协议的检测

我了解BQ24195之类的芯片可以使用BC1.2,但是由于我只有一个USB端口,所以没有采用

TI有没有与TPS2543之类的可以处理BC1.2检测的同时又能够将host和device连接起来,并且还支持双向输出的芯片呢?(2543是仅输出,无法辨别DFP的供电能力)

或者有什么更优的方案可以处理这个问题呢?

谢谢!