您好:
我目前使用TPS61175做升压,输入电源约8V,输出电压12V,最大电流约0.8A,目前带载功能均正常。测试该芯片的过流保护功能时,使用电子负载测试,输出电流设为5A,输出电压并没有变为0,而是5.5V,即使输出电流设为10A,输出电压也没有变为0,而是更低的电压。负载改为正常0.8A时,输出电压正常。如上附图为原理图及5A负载时的输入输出电压图。请问这现象是正常的吗?该芯片过载时的反应是什么呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我目前使用TPS61175做升压,输入电源约8V,输出电压12V,最大电流约0.8A,目前带载功能均正常。测试该芯片的过流保护功能时,使用电子负载测试,输出电流设为5A,输出电压并没有变为0,而是5.5V,即使输出电流设为10A,输出电压也没有变为0,而是更低的电压。负载改为正常0.8A时,输出电压正常。如上附图为原理图及5A负载时的输入输出电压图。请问这现象是正常的吗?该芯片过载时的反应是什么呢?
Hi
这个芯片的电流保护是cycle-by-cycle overcurrent limit ,并非lathc(关闭),所以电流保护不是拉低到0V, 而限制duty后输出电压被拉低。