This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3488: 可编程输出电压设计验证(SEPIC)

Part Number: LM3488
Other Parts Discussed in Thread: TIDA-010057

您好,

我在设计一个用LM3488实现的SEPIC直流升压电路, 整体在参考TIDA-010057。我这边希望做一个可以调节的输出电压,但是网上并没有实列。我根据TIDA的说明书进行了一些计算,能否麻烦您帮忙看一下假设及推导过程是否合理。以下照片为说明书的设计截图。

设计我的输出电压可调范围在15V~80V, 输入的控制电压在0V~5V。假设R1跟原设计一样是298kohm。那么R2和R3的值通过以下计算可得:

继而电路图是这样的:

麻烦您帮忙确认以下几点,非常感谢:

1. R2, R3 的阻值推导是否合理,最终电路图是否正确?

2. TIDA 文件中 figure 4-1 (以上图片中)并未明确说明Vref为多少。我认为它是LM3488的FB引脚的reference voltage。不知这个假设是否正确。

3. 在TIDA的figure 4-1中,Vadj对应的是我输入的控制电压(0~5V)吗?

4. 关于LM3488的FB引脚到地的阻值是否有最小值限制?根据我的设计它是6.02k ohm。