Other Parts Discussed in Thread: LM3409
您好,咨询下,我使用LM3409 DEMO的原理图设计,想设计输入12V,输出5V/2A,能否帮忙提供下图标上的参数配置,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,咨询下,我使用LM3409 DEMO的原理图设计,想设计输入12V,输出5V/2A,能否帮忙提供下图标上的参数配置,谢谢
Hi
可以按照datasheet 第28页的案例来计算相关参数即可。
输入9-16V,输出5V的情况下VTURN-ON这个值配置为多少合适?也是设计为10V吗?
另外,请教一下该电路是否适用于输入不是固定值而是一个范围,比如9-16V,均能固定输出5V?
Hi
设计到9V以下,例如8V.
可以的,输入9-16V,均能固定输出5V。
如果负载是一个PTC加热器,只有3欧姆左右,接到电路中无输出电压,请问需要调整哪些参数?谢谢!
HI
LM3409适合设计LED驱动, 应该是不适合接PTC负载的。