Other Parts Discussed in Thread: BQ40Z50
您好!
我现在遇到SOC计算不准确,在以6000W的功率放电,SOC在70%左右开始跳变同时RemC剩余容量也同步跳变,但是Passcharge的数据是正常,这份goldimage是延续已有正常的项目进行修改,ID等各方面都和前项目一致,唯一区别是放电功率变大,但是应用在这个项目上SOC计算就开始不准确。
1.请问放电功率的大小会对SOC的计算有影响嘛,正常放电期间电流大概在110A-150A,请问会是这个影响嘛?假如不是请问我该怎么排除去解决问题,为什么SOC会跳变,跳变较大后变为0,但是电池包还具有一部份放电能力
2.Cell Charge Voltage T1-T2、Cell Charge Voltage T2-T3、Cell Charge Voltage T3-T4设置为4100mv,同时Cell Taper Voltage设置为200mv,这样是否合理?留有余量是为了后期将电池包的电压进行修改。
3.假如我的电池包为锂电池最大电压为56V,假如现在电池包为54.88V,那么校准时采取56还是54.88V。
4.附件是放电时SOC跳变的数据,请参考

5.麻烦回复,感谢!