Other Parts Discussed in Thread: LM3409
请问LM3409Q输出的开路电压在规格书中没有说明,开路时测到的电压是43V,请问这个电压可以调吗?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
见datasheet 第21页描述:9.1.6 Output Overvoltage Protection Because the LM3409/09HV controls a buck current regulator, there is no inherent need to provide output overvoltage protection. If the LED load is opened, the output voltage will only rise as high as the input voltage plus any ringing due to the parasitic inductance and capacitance present at the output node. If a ceramic output capacitor is used in the application, it should have a minimum rating equal to the input voltage. Ringing seen at the output node should not damage most ceramic capacitors, due to their high ripple current rating.
所以这个电压没法调的。