Other Parts Discussed in Thread: TPS61196
如TPS61196 SPEC中所述,单通道的电流设置在50mA~400mA,请教最小值可以在50m以下吗?最小值可以到多少?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
可以的,用调光即可或者更低电流。如果满调光设置,也可以设置小一些。
HI
可以小于50mA, 但是会略微差一些,超出1.5%.