Other Parts Discussed in Thread: LMR54410
在选型表没找到一个合适的电源芯片,希望能推荐一个合适的。
输入电压:5V-10V
输出电压 :-10v到 - 5v
输出电流:>100ma即可。
外围电路最好简单点,效率高点。最好是LDO。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
LDO无法正压输出负压。
你是要做到输出-5~-10V可调,还是其范围内某个值即可?
Hi
建议用降压芯片来做,选择输入电压大于20V, 电流500mA的降压芯片都是可以的,输出可以选择不要外部补偿的芯片。
选择chargepump,带载越大,输出电压偏差会加大,例如输出-8V, 加载100mA, 可能偏差到-8.5A.