如图,目前是完全空载的状态,VOUT就焊了个MLCC,输入有10V 0.077A
目前现象是 Vref有5V输出,en脚手动飞线拉到了5V,示波器测量LL没有任何波形,BST脚有5V没有任何波动,VOUT和FB都是0V
芯片换了两颗都是同样问题,实在排不出问题了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如图,目前是完全空载的状态,VOUT就焊了个MLCC,输入有10V 0.077A
目前现象是 Vref有5V输出,en脚手动飞线拉到了5V,示波器测量LL没有任何波形,BST脚有5V没有任何波动,VOUT和FB都是0V
芯片换了两颗都是同样问题,实在排不出问题了
Hi
输入如果是10V, 输入电容建议至少44uF(2个22uF,或10uF+47uF) layout上尽量靠近Vin。、
REF电容也要加大,建议至少1uF。
已经加了电容,但还是没有任何输出。。。电感上也没有任何波形
调试的时候观察到TRIP引脚,在EN下拉(关闭)时是0V,EN拉到5V时能量到1.2V,应该能证明芯片没虚焊