This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: LM5122的反激应用请教

Part Number: LM5122
Other Parts Discussed in Thread: LM5155, PMP9256

你好,

我正在使用LM5122设计反激应用。遇到了一些问题,请教贵司团队。

问题1、我们功率上到60W以上时,表现出了次谐波振荡,LM5122的斜坡补偿是否无效?因为我看它是通过检测电感电流的下降斜率来得到补偿量

问题2、LM5155这种外部补偿的方案,是否更适合应用在50%占空比以上的应用;

我们的设计参数规格:Vin:5~28V  Vout:80~120V;20V输入以下限制输入电流最大3A,20V及以上最大输入电流5A;匝数比1:5,初级感值8uH;

期待得到您的回复!谢谢