Part Number: LM5122
Other Parts Discussed in Thread: LM5155, PMP9256
你好,
我正在使用LM5122设计反激应用。遇到了一些问题,请教贵司团队。
问题1、我们功率上到60W以上时,表现出了次谐波振荡,LM5122的斜坡补偿是否无效?因为我看它是通过检测电感电流的下降斜率来得到补偿量

问题2、LM5155这种外部补偿的方案,是否更适合应用在50%占空比以上的应用;
我们的设计参数规格:Vin:5~28V Vout:80~120V;20V输入以下限制输入电流最大3A,20V及以上最大输入电流5A;匝数比1:5,初级感值8uH;
期待得到您的回复!谢谢