This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: 在冲放电后,重启芯片SOC会跳变,每次出现不一样的值,假如在静置即电池是稳定的时候重启SOC基本不会变化

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: GPCRA0

Ti工程师,您好!

   1.如标题所说,在冲放电后,重启芯片SOC会跳变,每次出现不一样的值,假如在静置即电池是稳定的时候重启SOC基本不会变化,为什么出现这种情况,出现这种情况正常吗?假如不正常如何修改

   2.对于Avg P Last Run参数,是不是更新需要有时间限制,500-600S区间才会更新这个值,另外现在的机器放电功率较高,达不到这个放电时间,所以一直都不会更新。另外我尝试手动填充一个值,但是发现填充这个值和实际放电功率6000W,发现会把FCC变得很小3/4Ah,这是为什么?

   3.我现在以6000W的功率放电,发现把Cell Terminate Voltage从2400调为2600或者比2600大的时候会导致SOC从70%开始跳变,跳变几秒后变为0,为什么出现这种现象,该怎么修改?

   4.T Rise、T Time Constant跟电芯发热有关,那么这个变量会SOC的影响大嘛。我现在采用默认值,产品升温较快,6000W放电功率,假如要比这个因为考虑进去,那么该向上修改还是向下修改

5.麻烦回复,感谢!