This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: BQ25756的反向问题

Part Number: BQ25756
Other Parts Discussed in Thread: , BQ25750, BQ25750EVM

BQ25756与bq25756evm问题咨询:

1.看到BQ25756规格书中有描述反向模式功能,请问BQ25756EVM是否可以完成反向模式?如果不可以,想要实现反向功能应该如何实现?

2.BQ25756的反向模式是否也是可以达到正向模式一样的BULKBOOST模式到相应后级进行调节?

3.选择BQ25756的芯片是因为BQ25750一直处于缺货状态,BQ25750何时可以有货释放?

 

 


  • 感谢您对TI产品的关注!
    关于你的咨询,
    1. BQ25756EVM是基于BQ25756推荐电路设计的,是支持评价BQ25756的反向功能的。
    2. BQ25756的反向模式也是支持电压,电流调节。
    The device supports buck-boost reverse power direction to deliver power from the battery to the input when
    the adapter is not present. In reverse mode, the regulation voltage and current can be programmed via the I2C
    interface (VAC_REV and IAC_REV) to provide a CC/CV profile supporting the USB-PD Extended Power Range
    (EPR).
    更多信息,你可以在datsheet中搜索reverse mode,参阅跟多关于反向模式的技术信息。

    www.ti.com/.../bq25756.pdf

    3.对于货物的库存状态,建议您关注所需购买芯片的产品主页,库存以您登录TI.com后看到的为准,TI会实时更新库存情况。

    希望我的回答对你有所帮助。


  • 追问:

    4.BQ25750芯片的反向模式,是不是仅可以做BULK调整,做不到BOOST方式?因为在规格书中看到Vsysrev需要低于Vbat。

    5.根据BQ25750EVM里推荐的电路图,如果在反向模式中电池放电,通过转换器向Vsys引脚外进行放电,放电电流并没有经过Racres电阻,Iacrev电流还能被调节吗?或者问在反向模式中,Iacrev调节向外部Vsys引脚 的放电的电流采集电阻是哪个?

  • Datasheet提到有reverse boost mode。

    可以做到

  • 第5条问题,我用DEMO板测试过,电流不能被调节。不排除测试方式错误。