This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教bq51013b接电子负载动态CC模式OUT断掉问题

Other Parts Discussed in Thread: BQ51013B, BQ51020

测试条件:发送端TI 5V 1A无线发送端,接收端BQ51013BEVM-764,电子负载设置0mA-300mA两个状态动态切换,周期为200ms。

用示波器查看发现bq51013b的OUT端会不规律的断开,断开时间有长有短,长的30ms左右,短的5ms左右。断开后又自动连接,但接收端与发送端的通信没有断。所以发送端的供电是正常的。如果把动态电子负载切换周期设置为1s,则OUT端的断开现象会好很多,但仍有断开现象。

想请教下这个现象是不是因为BQ51013B的Adaptive Communication Limit功能引起的呢?如果是的话有避规办法吗?另外在BQ51013与BQ51020的接收端没有发现该问题。求助。谢谢。