This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951: 打嗝模式问题

Part Number: UCC28951
  • 在什么情况下UCC28951会触发打嗝模式,是否是同过芯片的某一个io在采集到信号的时候触发芯片的打嗝模式?
  • Hiccup mode. This mode provides overload protection to the power circuit. The UCC28951 controller stops switching after a certain time in current limit. It starts again (soft-start) after a delay time. The user can control the time spent in current limit before switching is stopped and the delay time before the soft start happens.

    The hiccup mode with the restart can be disabled by the user if a pullup resistor of 261 k Ω is connected between the SS and VREF pins. 

    详情请查看下方手册链接31页关于hiccup配置相关章节。

    https://www.ti.com/lit/ds/symlink/ucc28951.pdf#page=31