Other Parts Discussed in Thread: TPS62120, TPS62110-HT, TPS54062, TPS5401, TPS54040
TI技术工程师,您好!
我这里需要您帮忙推荐一款DC-DC电源IC。
要求:15V--3.3V,小功率(输出负载20mA),效率85%以上,耐高温(正常工作温度125°C)。
目前我们选用的是贵公司TPS62120,但是这款IC温度不太满足,故请帮忙再推荐一款。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS62110-HT - www.ti.com/.../tps62110-ht
Parametrics:
Iout (Max) (A) 1.5
Vin (Min) (V) 3.1
Vin (Max) (V) 17
Vout (Min) (V) 1.153
Vout (Max) (V) 16
Iq (Typ) (mA) 0.032
Switching Frequency (Typ) (kHz) 1000
Switch Current Limit (Typ) (A) 2.4
Topology Buck
Operating Temperature Range (C) -55 to 175
Pin/Package 16HTSSOP
Approx. Price (US$) 68.00 | 1ku
Rating Catalog
Duty Cycle (Max) (%) 100
Regulated Outputs (#) 1
如你所选TPS62120系列芯片是专门设计作为小电流输出的DC/DC芯片,所以效率可以达到很高85%,但是受到温度85℃的限制使得其不能工作在高温状态。另外有TPS54062,结温可以到达125℃,效率75%左右(20mA)
除这一类芯片之外的其他芯片,温度是可以到150℃(热保护在170℃以上),但是并非小电流输出的设计,所以效率一般都在50%左右,例如TPS5401, TPS54040等等。