This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25505: 芯片的选型问题

Part Number: BQ25505

请帮助选型,
要求
1.太阳能电池板输入电压:4.5V及以上(标准5V)
2.单节锂电池充电,标准锂电压3.6V,最大4.2V,充电电流500mA及以上。
3.具有MPPT功能
4.具有输入低压停机保护、充电、过流保护等保护功能。

每年有4KK的需求
特殊要求:
用于太阳能充电MPPT的充电IC。电池安装在充电IC上
POWer pass功能可用吗?如果我的充电芯片不工作,电池能为模块供电吗?模块的平均功耗为100-200mA,当功率高时,瞬时可以达到2-3A,
是否可以为系统提供2-3A的电源,无论其是否处于充电状态?

BQ25570RGRT、BQ25505RGRT、BS24650RVAR、TI-BQ25504、TI-BQ15505根据我的要求,选择哪种芯片最合适、最划算?