This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28742: 反激电源输出异常

Part Number: UCC28742

使用UCC28742设计3路输出反激电源,5V为反馈绕组(设计额定输出2A),调试过程中遇到两个问题

1.输出带额定载电源无法启动,轻载可以启动,启动后可以正常加载

2.启动后输出加载可以运行,但是持续运行几分钟后电源输出会掉,进入类似打嗝保护的重复启动状态,测量均未发现OC及OV故障

下图是Vds电压波形(时间刻度分辨率问题波形采集略失真),运行异常前占空比从正常50%变化到几乎100%,有人遇到过类似的问题吗,请帮忙提供解决简易,谢谢