Other Parts Discussed in Thread: LM43601
假设已经得到20V的直流电, 能输出1A电流。要把它变为电压可调的数控电源,调节范围1~18V, 电流至少500mA,变差小于200mV。
有什么大致方案吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM43601
假设已经得到20V的直流电, 能输出1A电流。要把它变为电压可调的数控电源,调节范围1~18V, 电流至少500mA,变差小于200mV。
有什么大致方案吗?
大致思路:
1.采用线性电源,热损耗会比较大,有限考虑使用开关电源。
2.可调电源为降压,有限考虑使用Buck,简单,好调。
3.要程控,无非就是改变BUCK的占空比。一般的Buck只有Feedback可以成为程控的输入。
4.Feedback既能接受输出的反馈,又要能接受用户的设定,因此这两个信号需要使用某种电路叠加。
5.叠加的方法有不少,最简单的可以使用两组串联的晶体管,另外还可以使用运放搭建简单的加法电路。
6.叠加之后,还需要数字控制,因此可以考虑使用DAC做精确的控制。如果DAC成本太高,可以使用PWM来简单的模拟之。
如此想下去,一个一个问题的解决,最终就可以设计出来啦~
祝楼主一切顺利!