This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25883EVM: Demo板测试下来的问题

Part Number: BQ25883EVM

1.目前测试上我这边有些疑惑,我这边测试JEITA的时候,将TS的电压调制cool和warm状态,发现充电电流没有变化,依旧是全程保持恒流充电,而我已经设置成40%ICHG,

2. JEITA功能测试,TS调节到cool和warm两种状态电压的时候,上位机设置为限流充电(40%ICHG),但是实际测试发现,在调节到这两种状态,限流并没有生效,依旧日是100%ICHG进行充电。
3.cool状态,电流限制为20%ICHG,芯片会陷入保护,停止充电。
设置为40%ICGH,电流比之不限制,仅仅下降了10%不到。如:设置为1A电流输入,稳压电源显示0.95A,电子负载显示0.649A。限制在40%,稳压电源显示0.87A,电子负载显示0.595A(高温设置在40%ICHG亦是如此。)

以上情况,请帮我分别看看什么问题,以及怎么解决,谢谢!