This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电源选型问题

Other Parts Discussed in Thread: TPS62173

Hi  Expert:

有一个项目,板子需要5V的直流电源,输入的是来自开关电源的12V直流,正常工作状况板子的电流100mA左右。 先是用了一片1117,发现烫的很厉害,工作十几分钟后都不能用手去摸,现在有几个问题,希望得到专家的指导: 1. 这种情况下,用1117有没有问题? 2. 如果不用1117,备选方案是2595和62173,如果用这两个片子,我在TI的WEBENCH软件中,输入的最大电流应该是多少?(0.1A还是留点裕量?如果留裕量,应该留到多少) 3. 2595的最大输出电流是1A,62173的最大输出电流是0.5A,我的板子0.1A的工作电流能够长期不断电的工作吗?因为在datasheet里面说低电流的时候工作在discontinuous模式,似乎不推荐。 4. 如果板子上还有模数转换芯片,推荐用什么样的电源芯片?

谢谢!