This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TS接10k欧姆还是100K欧姆,取决于你选择BQ24090这个系列芯片里的具体那一款,参考datasheet的page 4,如果是BQ24090 则接10K欧姆,如果是BQ24091则接100K欧姆,所以datasheet中说接10K/100K TS电阻,这个pin脚描述是针对这一系列芯片的,不是针对BQ24090这一款芯片的,注意datasheet 页眉上标注的器件型号。
6 Device Options(1)
PART NUMBER VO(REG) VOVP JEITA TS/CE PG PACKAGE
bq24090 4.20 V 6.6 V No 10 kΩ NTC Yes 10 PIN 5x3mm2
bq24091 4.20 V 6.6 V No 100 kΩ NTC Yes 10 PIN 5x3mm2
bq24092 4.20 V 6.6 V Yes 10 kΩ NTC Yes 10 PIN 5x3mm2
bq24093 4.20 V 6.6 V Yes 100 kΩ NTC Yes 10 PIN 5x3mm2
bq24095 4.20 V 6.6 V No 10 kΩ NTC Yes 10 PIN 5x3mm2
以上谢谢!
你好,
我电池包还要经过降压给系统供电。 可以回答我上面的问题吗
低成本BQ2000,高性能建议BQ24618 。
如果终端应用是移动电源,建议BQ24195系列。
你好,
是对四节并联的4*2600mAh锂电池(18650)充电,共10400mAh.
并联主要影响cc电流的选择,串联更麻烦一点需要考虑到CV以及电芯平衡。