This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930 IIC通信问题

Other Parts Discussed in Thread: BQ76930, BQ76930EVM

你好,我使用的芯片是BQ76930003ATG4C5ZC,使用了一块BQ76930EVM板和EV300,在上位机上显示的地址是0X08,电压数据正常,现在我自己写了一个IIC程序(是使用MCU的IIC接口,不是模拟IIC程序),硬件环境是使用一块8位的MCU芯片和BQ76930EVM,将EVM的IIC接口与MCU的IIC接口接上,两块板共地,拔掉了EVM板上J14上的所有跳帽,这个程序测试读写支持IIC协议的AT24C02的EEPROM芯片正常,但是现在不能读取到BQ76930的电压数据,我写的地址是0x10,读的地址是11,急待解决。初始化BQ769芯片的寄存器写入的地址add[11] ={0x00,0x01,0x02,0x04,0x05,0x06,0x07,0x08,0x09,0x0a,0x0b}; 在初始化寄存器中写入的配置数据data[11]={0x08,0x00,0x00,0x10,0x00,0x00,0x00,0x00,0xAC,0x97,0x19};写入和读取的程序模块,现在没有数据出来,REGOUT是4.5V

for(i=0;i<11;i++) {

WRITE_IIC(add[i],data[i]); 
delayms(5); 
}
delayms(250);
for(i=0;i<5;i++){

readbuf[i]=IIC_read_one_byte(regadd[i]);
delayms(5); 
}