This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: 电池在接近满电状态下,其RSOC、剩余容量、FCC皆为0,内阻表异常

Part Number: BQ34Z100-G1


4串3元锂电池在接近满电状态下(电压为16.5V),电量计上报的RSOC、剩余容量、FCC出现异常情况,皆为0,且SOH为80%;

查看内阻表,发现2份内阻表差异很大,相差7倍;

插入充电器充电直至充满,RSOC由0%跳变至100%,剩余容量为10.197Ah,FCC为10.951Ah,SHO为96%,上报的容量低容,电池最低容量为14.5Ah;

异常电池按0.2C做标准充放电循环,期间Log数据并查看内阻表,发现数据皆正常,0.2C放电精度误差都<3%;

已上传相关异常现象图片、异常配置文件和测试数据;

麻烦分析下原因,谢谢!

B0859-客退异常电池-初始配置.gg.csv   B0859-客退异常电池-充放电循环后配置.gg.csvB0859-客退异常电池-0.2C充放电数据.csv