This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: When applied to a 4S battery board, how should the regin pin be connected?

Part Number: BQ35100

Dear All,

When I want to use BQ35100 in a 4S1P circuit
How do I connect the regin pin?
Because I see that the REGIN PIN can only withstand 5.5V.
Is there any reference connection method? Is it necessary to add LDO?

Thanks!