1、问题描述
输出电压纹波偏大,24V转12V输出,0A时纹波电压116mV;1.5A时纹波电压434mV,如下图。
图1 图2
2、电路原理图如下图。
图3
3、PCB布局如下图。
图4
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您对TI产品的关注!
关于你的咨询,你调整下输出电感值和电容值。
电感值15uH小了,换个27uH的看下。
另外,还跟你的布局走线有关系。
datasheet的8.4 Layout章节有pcb layout设计指南,你看看是否遵循了建议。
你也可以参考下TPS54531评估板的layout设计。
www.ti.com.cn/.../zhcuad6