This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TPS54550 带载后电压异常,求大神



输入电压5V(电流3~4A),输出为-5V,输出用水泥电阻做模拟负载,L1为22uH 4A的SMD 带磁芯功率电感。

空载时,输入电压4.98V,输出电压-4.95V;

负载3R时,输入电压4.98V,输出电压-4.92V;

负载2R时,输入电压4.98V,输出电压约-1.3V;

负载2R时,输入电压12V,输出电压约-4.93V;

需要的是,输入电压5V,输出电压-5V,输出电流至少3A,求大神指点,是哪里有问题