附近中所示的电路,当取下MOS管,输入10v-30v时,驱动MOS的电压都有7V。
但焊接上MOS管后,带负载1A时。输入10v时,驱动电压只有4.2V,输入15v时驱动电压只有3.4V,且随着输入电压的升高,mos驱动电压反而会降低。mos用的是FDD8447L,换过其他的也一样的结果。
求解,这是为什么呢?驱动电压怎么没有7V呢?驱动电压太低了不行啊
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
见datasheet : www.ti.com.cn/.../lm3478.pdf 第八页,驱动电压定义:The voltage on the drive pin, VDR is equal to the input voltage when input voltage is less than 7.2V. VDR is equal to 7.2V when the input voltage is greater than or equal to 7.2V. 也就是是说驱动电压的大小与Vin的大小相关。
电源转换时,输入电压会因为负载输出而被拉低然后在被输入补充,所以输入会形成纹波,为了减小输入电压被拉低,输入都是需要增加电容的,在您的设计中,输入电容是够的,layout上可能存在问题,您用示波器测试一下芯片脚Vin的电压波形,即可得到结论。在这种情况下您可以在芯片脚上(尽量靠近Vin脚)上焊接一个10uF~47uF的电容(以实验结果为准), 在后续的layout中需要注意输入电容尽量靠近芯片(Vin,输入的trace也尽量宽一点。
合理的解释是:你用万用表来测量驱动电压! 输入电压升高,咱空比变小,万用表的读数为积分值。
请用示波器测量。